Please find the below design requirement and I have selected the TPS76525 power regulator device
Design Requirement:
Input Voltage – 3.3V(9%)
Output Volatage – 2.5V(9%)
Output Current – 50.4mA
Total Capacitance in that rail - 55uf
In datasheet, they have given the minimum required output capacitor is 4.7uf. But there is no maximum cap requirement is given. Can I use maximum capacitor value as 60uf with meeting the specified ESR value. Is that ok?. Please confirm for finalizing the component or suggest any other alternate devices with “POWER GOOD and ENABLE” pins.
Thanks & Regards,
Jeyalakshmi Kanniah