This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fuel gauge - how to manage sudden heavy load ? is special battery monitoring algorithm needed in application layer ? or it can be controlled in hardware side?



hello all ,

           we are using  our custom board with DM385 which is battery powered. we are facing an critical issue on battery monitoring side .  on ideal state our board was consuming  0.44 watts ( 3.7v * 120mA). but when our device starts streaming the video, power consumption was  around 1.85w (3.7v * 500mA) .  

          we want to show the battery percentage in application layer with datas from fuel gauge .  since  difference between  our  power consumption on ideal state and  full streaming state was  1.4 w ( 1.85w -0.44w) , the percentage on GUI was falling and rising with huge difference.   

1. How to deal this ? is it really a problem on s/w or h/w or its normal with this kind of power difference ?  How to deal this ?


         Pmic and charger we are using were from TI but  our fuel gauge was not from TI . it was from some third party having following  two modes of operation

1.Voltage mode ( gives capacity only with voltage)
2.Mixed mode  ( gives capacity with both voltage and current)

   2. we are not getting the current values updated in our fuel gauge ,so mixed mode of operation is not working  but voltage mode is working good with correct voltage values . we are working on to make mixed mode of operation working.  is current and voltage combination for calculating capacity will solve this issue of huge power consumption difference? we think it will not !! . we are not getting proper support from fuel gauge vendor ! .   we expecting your valuable  suggestion .
   


   

  • Hello,

    This question really depends on the size of the battery.

    In order to further guide you, may I ask the following:
    1. What is the capacity of your battery?
    2. When it was created by the cell maker, does it have high discharge rate properties?

    Texas Instruments has voltage only gas gauges and also voltage/current gas gauges that are very advanced to handle different types of dynamic loads. Would you like to take the conversation offline in order for us to dig a little deeper into your battery and system?

    Thanks,
    Kang Kang
  • Hai kang kang,
    sorry for late reply. below are the details you asked for
    1. 1400mAh
    2. manufacturing date was not provided by the vendor but it will work with full functionality upto < 300 cycles of charging and
    discharging approximately.
    and as per the datasheet it can discharge at
    standard - 0.5C
    MAX - 1C in contineous discharging

    and i am very thankfull to have offline conversation with you .