I have a 4S1P pack with 3400mAh 18650 batteries. I am trying to test the cell balancing feature. I noticed that most of the reference designs have a 100 Ohm resistor into the Vx pins of the BQ3050. If I have a 4V cell, and I read that the Rdson of the bypass FET is 125 Ohms, the 100 Ohm resistor would produce a current around 16mA. This exceeds the 10mA max current for this pin. I am not seeing much response when the Cell Balancing flag is active, but 10mA is not much compared to the 1500mA of charging current. I am wondering if I damage the part by using the 100 ohm resistors and that is why it is not seeming to work, or is the current so low compared to the charging current that it does not make a difference.
Will it take many charge/discharge cycles to balance something like a 200mV cell difference? We try to match them within 10mV when installing but sometimes my customers do bad things like remove the batteries from a few units and then put them back randomly.
Thank you,
Richard