Hi,
I am doing a project on wireless charging using the BQ500412, where I am trying to implement the coil on the PCB as trace inductance.
Under the A6 guideline, the inductance on the PCB needs to be 12.5uH for 1 coil. I need to carry out simulations to ensure that the right power is being outputted. Could I please get the input waveform to the coils in BQ500412 from the Power Mosfet ?
Also, is there another way for me to drive the coil instead of using the recommended Power Mosfet in order to make the circuitry simpler?
Kind regards,
Kanav Batra