Hi!
I am using the LMZ10505 part, but I am experiencing several failures after solder reflowing.
Due to some ROHS FPGA's, the reflow temperatures for the board reaches approximately 260C. Unfortunately, the maximum reflow temperatutre for the LMZ10505 is 245C, which is why some fail afterwards.
Does anyone have a recommended replacement part with the same (or similar) package but higher (ideally > 260C) reflow temp limit?
The power rails are:
- Vin: 5 to 5.5V
- Vout: 3.3, 2.5, 1.8 and 1.0V
- Iout: 1, 3 and 4A depending on the design.
Thanks,
James