Hi,
I am using USB to GPIO to reprogram power manager IC available on Xilinx ML605 board
I am getting these errors
11:44:27.016 |
CUSTOMER |
GENERAL |
Summary |
Percentage pass: 5.1 %, Percent difference: 99 % |
11:44:27.016 |
CUSTOMER |
ERROR |
Summary |
READ_VOUT on rail #1 (0.010 V) was not within 5.1% of VOUT_COMMAND (1.000 V) |
11:44:27.047 |
CUSTOMER_LOGONLY |
ERROR |
Summary |
READ_VOUT on rail #1 (0.010 V) was not within 5.1% of VOUT_COMMAND (1.000 V) at TIDP.Factory.TaskLibrary.UCD9240.Validate_Vout_Device_Reading(Int32 rail_num, Double percent_pass) in C:\Anne_TI\Workspaces\FusionTools-Main-B\Libraries\TIDP\TIDP.Factory.TaskLibrary\UCD9240.cs:line 548 at TIDP.Factory.TaskLibrary.UCD9240.Validate_Vout_Device_All_Rails(Double percent_pass) in C:\Anne_TI\Workspaces\FusionTools-Main-B\Libraries\TIDP\TIDP.Factory.TaskLibrary\UCD9240.cs:line 596 |
11:44:27.063 |
CUSTOMER |
GENERAL |
none |
[message] Title:Failure occured... - Prompt: READ_VOUT on rail #1 (0.010 V) was not within 5.1% of VOUT_COMMAND (1.000 V) |
Please Help me out
Regards
Yatindra K Trivedi