This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq25505

Other Parts Discussed in Thread: BQ25505

Trying to charge NiMH cells with the bq25505. Using four (4) NiMH cells in series requires charging a bit higher than the 5.5V maximum of the part so I'm worried about long-term damage to the part. Has anyone used the 25505 (or other parts in the family) to charge NiMH cells? (

Also, since I'm using 4 NiMH cells, I have 4 alkaline cells for the backup power source which is switched in when the NiMH cells are depleted. Four new Alkaline cells can exceed 6V total so is that another problem I need to consider?)