Hi there.
We are designing a buck with TPS54521. Fixed Input 12V, and Output requirement is 5V/4A. We have to estimate the junction temprature to prevent overheat.
As simulated in WEBENCH, the efficiency is about 90%, so the power dissipation Pd=(5V*4A/0.9)*(1-0.9) = 2.22W. Assume the environment temperature Ta=25 degree. When I read thermal parameters on page 3 of datasheet, my questions are :
(1) why there are two θJA? one is 47.2 and another is 32 ? what's the difference?
(2) Which parameter should I use to estimate the junction temperatur? θJA or θJB? some one suggest using Tj=Ta+Pd*θJA, that seems reasonable, but I noticed that TPS54521's PowerPad is helpful to dissipate heat, since the thermal resistance of juction-to-board θJB is just 3.2 degree/watt, much less than θJA.
(3) According to datasheet, these thermal parameters are tested under certain conditions. How will these parameters change when it comes to the real product?
I am confused about this situation. Does TI has any learning material that can help me understand these thermal parameters and give some guidacne to make reasonable estimation in thermal management ?
Thanks a lot!