Hi Everyone,
I'm looking for a solution that can fuel gauge a 4 Series Cell LiPo battery (10000mAh, 14.8V) and report pack information over SMBus or I2C. However the battery is removable and will be charged externally, furthermore the cell taps are not accessible.
I've been looking through the battery fuel gauges and datasheets and the system side Impedance track fuel gauges took to be ideal, except for the 1,1-2, cell Limitations. The bq78PL114, bq20z** (60, 75, 90, 95) also looks promising, but the cell tabs are not easily accessible.
I was wondering if a solution exists to my requirements? Would the flash based fuel gauges work or am I going to have to get access to the series cell taps?
Thanks,
Tom.