This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3492 Design and Eval Board Behaving Erratic

Other Parts Discussed in Thread: LM3492

So my company is working on a product requiring high power LEDs and selected the LM3492 as the best option. Our application is for two strands of two 6V LEDs and 100mA through each strand. After following the guide to part selection, a board was made and ordered, and did not work. On first power up, lights remained off and the IC quickly began heating up. Second attempt (with same board) gave a brief flash to one strand before shutting down. As no one here has experience with this chip, we ordered the evaluation board to observe how a working circuit behaves. From the data sheet, it appears that the eval circuit should work with our LED strands so we used them instead of 10 LED strands as described in the sheet. During the setup procedure for the eval board (Step 4, connecting DIM1 + DIM2 to >2V) suddenly only strand 2 powered up drawing over 500mA even though the circuit has a 150mA limit. What makes it weirder is that grounding the enable pin gives the same result; no shutdown. I am at a loss as to what is going on here, anyone have suggestions on what to try to get this thing operational?

Thanks,

  • Michael:
    When you use the LM3492 EVM, please follow the user's guide. The input voltage range is 9 to 16V, the LED string voltage is 39V ( it can be off by a few voltages ). The two LED strings should have the same number of LEDs. DIM1 and DIM2 pins need to be connected > 2V.
    When you see 500mA current through the LED, that means the IC probably has already been damaged. Please replace the IC and try agian. The DIM1 and DIM2 pins need to be high before power up.
    David Zhang