Hi all:
I made a design using LM3409, following one of the example design in the datasheet.
It has been designed with the following parameters and components:
Vin=44, Vout=29.2V, I=4.5 A, Enable pin : dimming at 15 Hz, Iadj pin totally Open. With those requeriment, I put
Roff:33k
Coff:470 pF
Ruv1:6.98k
Ruv2:49.9k
Cin:56uF
Cf:1uf
Rsns:50mohm
L1:22uH
Cout:none
I have made my circuit calculating 4.5 A , But I only get about 3A. Leds string can reach 5 A pulsed
I have recalculate the components values, but it seems correct. Do everyone have the same problem, or the expected intensity value is aproximately the same tan the one you get in the real circuit? I am quite confusing about which componets influences these values or what is the problem in the desing or component selection to get 1.5 volts less that expected.
I am thinking in the PFEt, that has a ver high RDsON (280 mOhm) or L1, but I dont really know why.
Any help about what can I check could be very usefull
Best regards