Hi,
There are two pages (pages 38 and 40) in the TLV707 datasheet (regarding the DQN package) that are almost identical with just a slight difference in the dimension of the central pad (0.48mm vs 0.50mm). I cannot find any information in the datasheet that let me know which one I should I consider for the TLV70712PDQNR product (I understand that the difference in dimensions are very small but still curious as why there are two set of information there).
Could you help me to understand the differences between pages 38 and 40 (and also 39, 41)?
Thanks