This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sample Code for BQ24251

Other Parts Discussed in Thread: BQ24251

Looking for any sample code to help me get started on the BQ24251 charger.

  • /*
     * BQ24250 Battery Charger Driver
     *
     * Copyright (C) 2013,  Texas Instruments Corporation
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     */
    
    #include <linux/err.h>
    #include <linux/kernel.h>
    #include <linux/module.h>
    #include <linux/init.h>
    #include <linux/interrupt.h>
    #include <linux/i2c.h>
    #include <linux/power_supply.h>
    #include <linux/power/bq24250-charger.h>
    #include <linux/regmap.h>
    
    /* Registers */
    #define BQ24250_STATUS_CONTROL_REG	0x00
    #define BQ24250_CONTROL_REG		0x01
    #define BQ24250_BATTERY_VOLTAGE_REG	0x02
    #define BQ24250_TERM_CURR_CHARG_REG	0x03
    #define BQ24250_VIN_DPM_REG		0x04
    #define BQ24250_TIMER_NTC_MONITOR_REG	0x05
    #define BQ24250_VOVP_FRC_BATDET_PTM_REG	0x06
    
    /* STATUS_CONTROL Reg */
    #define BQ24250_WD_FAULT	BIT(7)
    #define BQ24250_WD_EN		BIT(6)
    #define BQ24250_STATUS		(BIT(5) | BIT(4))
    #define BQ24250_STATUS_MASK	0x03
    #define BQ24250_STATUS_SHIFT	0x4
    #define BQ24250_FAULT		(BIT(3) | BIT(2) | BIT(1) | BIT(0))
    #define BQ24250_FAULT_MASK	0x0F
    
    /* CONTROL Reg */
    #define BQ24250_RESET		BIT(7)
    #define BQ24250_IIN_LIMIT	(BIT(6) | BIT(5) | BIT(4))
    #define BQ24250_EN_STAT		BIT(3)
    #define BQ24250_TERM_EN		BIT(2)
    #define BQ24250_CE		BIT(1)
    #define BQ24250_HZ_MODE		BIT(0)
    
    /* BATTERY_VOLTAGE Reg */
    #define BQ24250_BATTERY_VOLTAGE		\
    			(BIT(7) | BIT(6) | BIT(5) | BIT(4) | BIT(3) | BIT(2))
    #define BQ24250_BATTERY_VOLTAGE_MASK	0xFC
    #define BQ24250_BATTERY_VOLTAGE_SHIFT	0x2
    #define BQ24250_USB_DET		(BIT(1) | BIT(0))
    #define BQ24250_USB_DET_MASK	0x03
    
    /* CURR_TERM_CHARG Reg */
    #define BQ24250_CHARGE_CURR	(BIT(7) | BIT(6) | BIT(5) | BIT(4) | BIT(3))
    #define BQ24250_CHARGE_CURR_MASK	0x1f
    #define BQ24250_CHARGE_CURR_SHIFT	0x3
    #define BQ24250_TERM_CURR	(BIT(2) | BIT(1) | BIT(0))
    #define BQ24250_TERM_CURR_MASK	0x7
    
    /* VIN_DPM Reg */
    #define BQ24250_LOOP_STATUS	(BIT(7) | BIT(6))
    #define BQ24250_LOOP_STATUS_SHIFT	0x5
    #define BQ24250_LOW_CHG		BIT(5)
    #define BQ24250_DPDM_EN		BIT(4)
    #define BQ24250_CS_STATUS	BIT(3)
    #define BQ24250_VIN_DPM		(BIT(2) | BIT(1) | BIT(0))
    
    /* TIMER_NTC_MONITOR Reg */
    #define BQ24250_2X_TMR_EM	BIT(7)
    #define BQ24250_TMR		(BIT(6) | BIT(5))
    #define BQ24250_TMR_SHIFT	0x5
    #define BQ24250_TMR_MASK	0x3
    #define BQ24250_TMR_DISABLE	0x3
    #define BQ24250_SYSOFF		BIT(4)
    #define BQ24250_TS_EN		BIT(3)
    #define BQ24250_TS_FAULT	(BIT(2) | BIT(1) | BIT(0))
    #define BQ24250_TS_MASK		0x7
    
    /* Vovp_FRC_BATDET_PTM_REG */
    #define BQ24250_VOVP		(BIT(7) | BIT(6) | BIT(5))
    #define BQ24250_VOVP_SHIFT	0x5
    #define BQ24250_CLR_VDP		BIT(4)
    #define BQ24250_FRC_BATDET	BIT(3)
    #define BQ24250_FRC_PTM		BIT(2)
    
    #define BQ24250_MAX_REGISTER	0x6
    
    static struct reg_default bq24250_reg_defs[] = {
    	{0, 0x00},
    	{1, 0x2C},
    	{2, 0x8F},
    	{3, 0x00},
    	{4, 0x06},
    	{5, 0xA8},
    	{6, 0xD0},
    };
    
    enum bq24250_charge_fault {
    	BQ24250_NORMAL = 0,
    	BQ24250_INPUT_OVP,
    	BQ24250_INPUT_UVLO,
    	BQ24250_SLEEP,
    	BQ24250_BATTERY_TS_FAULT,
    	BQ24250_BATTERY_OVP,
    	BQ24250_THERMAL_SHUTDOWN,
    	BQ24250_TIMER_FAULT,
    	BQ24250_NO_BATTERY_CONNECTED,
    	BQ24250_ISET_SHORT,
    	BQ24250_LDO_SHORT,
    	BQ24250_MAX_CHG_FAULT,
    };
    
    static const char *desc[BQ24250_MAX_CHG_FAULT] = {
    	[BQ24250_NORMAL] = "NORMAL",
    	[BQ24250_INPUT_OVP] = "INPUT OVP",
    	[BQ24250_INPUT_UVLO] = "INPUT UVLO",
    	[BQ24250_SLEEP] = "SLEEP",
    	[BQ24250_BATTERY_TS_FAULT] = "BATTERY TS FAULT",
    	[BQ24250_BATTERY_OVP] = "BATTERY OVP",
    	[BQ24250_THERMAL_SHUTDOWN] = "THERMAL SHUTDOWN",
    	[BQ24250_TIMER_FAULT] = "TIMER FAULT",
    	[BQ24250_NO_BATTERY_CONNECTED] = "NO BATTERY CONNECTED",
    	[BQ24250_ISET_SHORT] = "ISET SHORT",
    	[BQ24250_LDO_SHORT] = "LDO SHORT",
    };
    
    #define BQ24250_DCP_DETECTED	0	/* dedicated charger */
    #define BQ24250_CDP_DETECTED	1	/* charging downstream */
    #define BQ24250_SDP_DETECTED	2	/* standard downstream */
    #define BQ24250_ACA_DETECTED	4	/* non-standard adaptor */
    
    /**
     * struct bq24250_charger - bq24250 charger instance
     * @dev: pointer to device
     * @regmap: pointer to driver regmap
     * @mains: power_supply instance for AC/DC power
     * @usb: power_supply instance for USB power
     * @battery: power_supply instance for battery
     * @mains_online: is AC/DC input connected
     * @usb_online: is USB input connected
     * @charging_enabled: is charging enabled
     * @pdata: pointer to platform data
     * @irq: fault irq number
     */
    struct bq24250_charger {
    	struct device		*dev;
    	struct regmap		*regmap;
    	struct power_supply	mains;
    	struct power_supply	usb;
    	struct power_supply	battery;
    	bool			mains_online;
    	bool			usb_online;
    	bool			charging_enabled;
    	bool			vsysoff_enabled;
    	int                     irq;
    	const struct bq24250_charger_platform_data *pdata;
    };
    
    /* Charge current in mA */
    static const unsigned int cc_tbl[] = {
    	500,
    	550,
    	600,
    	650,
    	700,
    	750,
    	800,
    	850,
    	900,
    	950,
    	1050,
    	1100,
    	1150,
    	1200,
    	1250,
    	1300,
    	1350,
    	1400,
    	1450,
    	1500,
    	1550,
    	1600,
    	1650,
    	1700,
    	1750,
    	1800,
    	1850,
    	1900,
    	1950,
    	2000,
    	0000,
    };
    
    /* Termination current in mA */
    static const unsigned int tc_tbl[] = {
    	50,
    	75,
    	100,
    	125,
    	150,
    	175,
    	200,
    	225,
    };
    
    /* Input current limit in mA */
    static const unsigned int icl_tbl[] = {
    	100,
    	150,
    	500,
    	900,
    	1500,
    	2000,
    	0000, /* For External ILIM current limit */
    	1111, /* No input current limit with internal clamp at 3A (PTM MODE) */
    
    };
    
    /* Battery Regulation Voltage in mV */
    static const unsigned int brv_tbl[] = {
    	0,
    	20,
    	40,
    	60,
    	80,
    	100,
    	120,
    	140,
    	160,
    	180,
    	200,
    	220,
    	240,
    	260,
    	280,
    	300,
    	320,
    	340,
    	360,
    	380,
    	400,
    	420,
    	440,
    	460,
    	480,
    	500,
    	520,
    	540,
    	560,
    	580,
    	600,
    	620,
    	640,
    	660,
    	680,
    	700,
    	720,
    	740,
    	760,
    	780,
    	800,
    	820,
    	840,
    	860,
    	880,
    	900,
    	920,
    	940,
    };
    
    /* Safety timer time limit in minutes */
    static const unsigned int stl_tbl[] = {
    	45,
    	360,
    	540,
    	0,
    };
    
    /* OVP voltage in mV */
    static const unsigned int ovp_tbl[] = {
    	6000,
    	6500,
    	7000,
    	7500,
    	8000,
    	8500,
    	9000,
    	9500,
    	10000,
    	10500,
    };
    
    /* Convert register value to current using lookup table */
    static int hw_to_current(const unsigned int *tbl, size_t size, unsigned int val)
    {
    	if (val >= size)
    		return -EINVAL;
    	return tbl[val];
    }
    
    /* Convert current to register value using lookup table */
    static int current_to_hw(const unsigned int *tbl, size_t size, unsigned int val)
    {
    	size_t i;
    
    	for (i = 0; i < size; i++)
    		if (val < tbl[i])
    			break;
    	return i > 0 ? i - 1 : -EINVAL;
    }
    
    /**
     * bq24250_update_ps_status - refreshes the power source status
     * @bq24250: pointer to bq24250 charger instance
     *
     * Function checks whether any power source is connected to the charger and
     * updates internal state accordingly. If there is a change to previous state
     * function returns %1, otherwise %0 and negative errno in case of errror.
     */
    static int bq24250_update_ps_status(struct bq24250_charger *bq24250)
    {
    	bool usb = false;
    	bool dc = false;
    	unsigned int val;
    	int ret;
    
    	ret = regmap_read(bq24250->regmap, BQ24250_VIN_DPM_REG, &val);
    	if (ret < 0)
    		return ret;
    
    	/*
    	 * DC and usb are set depending on whether they are enabled in
    	 * platform data _and_ whether corresponding undervoltage is set.
    	 */
    	if (bq24250->pdata->use_mains)
    		dc = !(val & BQ24250_DPDM_EN);
    	if (bq24250->pdata->use_usb)
    		usb = !(val & BQ24250_CS_STATUS);
    
    	ret = bq24250->mains_online != dc || bq24250->usb_online != usb;
    	bq24250->mains_online = dc;
    	bq24250->usb_online = usb;
    
    	return 0;
    }
    
    enum power_supply_property bq24250_charger_properties[] = {
    	POWER_SUPPLY_PROP_ONLINE,
    	POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT,
    	POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE,
    };
    
    static int bq24250_update_usb_type(struct bq24250_charger *bq24250)
    {
    	int ret;
    	unsigned int type;
    
    	ret = regmap_read(bq24250->regmap, BQ24250_BATTERY_VOLTAGE_REG, &type);
    
    	if (ret < 0)
    		return ret;
    
    	type &= BQ24250_USB_DET_MASK;
    	
    	switch (type) {
    	case BQ24250_DCP_DETECTED:
    		bq24250->usb.type = POWER_SUPPLY_TYPE_USB_DCP;
    		break;
    	case BQ24250_CDP_DETECTED:
    		bq24250->usb.type = POWER_SUPPLY_TYPE_USB_CDP;
    		break;
    	case BQ24250_SDP_DETECTED:
    		bq24250->usb.type = POWER_SUPPLY_TYPE_USB;
    		break;
    	case BQ24250_ACA_DETECTED:
    		bq24250->usb.type = POWER_SUPPLY_TYPE_USB_ACA;
    		break;
    	default:
    		bq24250->usb.type = POWER_SUPPLY_TYPE_UNKNOWN;
    		break;
    	}
    
    	return 0;
    }
    
    
    /*
     * bq24250_is_ps_online - returns whether input power source is connected
     * @bq24250: pointer to bq24250 charger instance
     *
     * Returns %true if input power source is connected. Note that this is
     * dependent on what platform has configured for usable power sources. For
     * example if USB is disabled, this will return %false even if the USB cable
     * is connected.
     */
    static bool bq24250_is_ps_online(struct bq24250_charger *bq24250)
    {
    	return bq24250->usb_online || bq24250->mains_online;
    }
    
    /**
     * bq24250_charging_status - returns status of charging
     * @bq24250: pointer to bq24250 charger instance
     *
     * Function returns charging status.
     * %0 means ready, %1 charging is in progress,
     * %2charging done and %3 fault.
     */
    static int bq24250_charging_status(struct bq24250_charger *bq24250)
    {
    	unsigned int val;
    	int ret;
    
    	if (!bq24250_is_ps_online(bq24250))
    		return 0;
    
    	ret = regmap_read(bq24250->regmap, BQ24250_STATUS_CONTROL_REG, &val);
    	if (ret < 0)
    		return 0;
    
    	val >>= BQ24250_STATUS_SHIFT;
    	val &= BQ24250_STATUS_MASK;
    
    	return val;
    }
    
    static int bq24250_vsysoff_set(struct bq24250_charger *bq24250, bool enable)
    {
    	int ret = 0;
    
    	if (bq24250->pdata->enable_control != BQ24250_CE) {
    		dev_dbg(bq24250->dev, "vsys enable/disable in SW disabled\n");
    		return 0;
    	}
    
    	if (bq24250->vsysoff_enabled != enable) {
    		ret = regmap_update_bits(bq24250->regmap,
    					 BQ24250_TIMER_NTC_MONITOR_REG,
    					 BQ24250_SYSOFF, enable ? 0 : 1);
    		if (!ret)
    			bq24250->vsysoff_enabled = enable;
    	}
    	return ret;
    }
    
    static inline int bq24250_vsystem_enable(struct bq24250_charger *bq24250)
    {
    	return bq24250_vsysoff_set(bq24250, false);
    }
    
    static inline int bq24250_vsystem_disable(struct bq24250_charger *bq24250)
    {
    	return bq24250_vsysoff_set(bq24250, true);
    }
    
    static int bq24250_timer_suspend(struct bq24250_charger *bq24250)
    {
    	int ret = 0;
    
    	if (bq24250->pdata->enable_control != BQ24250_CE) {
    		dev_dbg(bq24250->dev, "vsys enable/disable in SW disabled\n");
    		return 0;
    	}
    
    	ret = regmap_update_bits(bq24250->regmap, BQ24250_TIMER_NTC_MONITOR_REG,
    				 BQ24250_TMR, BQ24250_TMR_DISABLE);
    	if (!ret)
    		dev_err(bq24250->dev, "failed to suspend timer\n");
    
    	return ret;
    }
    
    static int bq24250_timer_reset(struct bq24250_charger *bq24250)
    {
    	int ret;
    	unsigned int tmr;
    
    	if (bq24250->pdata->enable_control != BQ24250_CE) {
    		dev_dbg(bq24250->dev, "vsys enable/disable in SW disabled\n");
    		return 0;
    	}
    
    	/* Reset with previous time value, when fault occur */
    	ret = regmap_read(bq24250->regmap, BQ24250_TIMER_NTC_MONITOR_REG, &tmr);
    
    	tmr >>= BQ24250_TMR_SHIFT;
    	tmr &= BQ24250_TMR_MASK;
    
    	ret = regmap_update_bits(bq24250->regmap, BQ24250_TIMER_NTC_MONITOR_REG,
    				 BQ24250_TMR, tmr);
    	if (!ret)
    		dev_err(bq24250->dev, "failed to reset timer\n");
    
    	return ret;
    
    }
    
    static int bq24250_charging_set(struct bq24250_charger *bq24250, bool enable)
    {
    	int ret = 0;
    
    	if (bq24250->pdata->enable_control != BQ24250_CE) {
    		dev_dbg(bq24250->dev, "charging enable/disable in SW disabled\n");
    		return 0;
    	}
    
    	if (bq24250->charging_enabled != enable) {
    		ret = regmap_update_bits(bq24250->regmap, BQ24250_CONTROL_REG,
    					 BQ24250_CE, enable ? 0 : 1);
    		if (!ret)
    			bq24250->charging_enabled = enable;
    	}
    	return ret;
    }
    
    static inline int bq24250_charging_enable(struct bq24250_charger *bq24250)
    {
    	return bq24250_charging_set(bq24250, true);
    }
    
    static inline int bq24250_charging_disable(struct bq24250_charger *bq24250)
    {
    	return bq24250_charging_set(bq24250, false);
    }
    
    static int bq24250_start_stop_charging(struct bq24250_charger *bq24250)
    {
    	int ret;
    
    	/*
    	 * Depending on whether valid power source is connected or not, we
    	 * disable or enable the charging. We do it manually because it
    	 * depends on how the platform has configured the valid inputs.
    	 */
    	if (bq24250_is_ps_online(bq24250)) {
    		ret = bq24250_charging_enable(bq24250);
    		if (ret < 0)
    			dev_err(bq24250->dev, "failed to enable charging\n");
    	} else {
    		ret = bq24250_charging_disable(bq24250);
    		if (ret < 0)
    			dev_err(bq24250->dev, "failed to disable charging\n");
    	}
    
    	return ret;
    }
    
    static int bq24250_set_charge_current(struct bq24250_charger *bq24250)
    {
    	int ret;
    
    	if (bq24250->pdata->max_charge_current) {
    		ret = current_to_hw(cc_tbl, ARRAY_SIZE(cc_tbl),
    				    bq24250->pdata->max_charge_current);
    
    		if (ret < 0)
    			return ret;
    
    		ret = regmap_update_bits(bq24250->regmap,
    					 BQ24250_TERM_CURR_CHARG_REG,
    					 BQ24250_CHARGE_CURR, ret);
    
    		if (ret < 0)
    			return ret;
    	}
    
    	if (bq24250->pdata->termination_current) {
    		ret = current_to_hw(tc_tbl, ARRAY_SIZE(tc_tbl),
    				    bq24250->pdata->termination_current);
    		if (ret < 0)
    			return ret;
    
    		ret = regmap_update_bits(bq24250->regmap,
    					 BQ24250_TERM_CURR_CHARG_REG,
    					 BQ24250_TERM_CURR, ret);
    
    		if (ret < 0)
    			return ret;
    	}
    
    	return 0;
    }
    
    static int bq24250_set_current_limits(struct bq24250_charger *bq24250)
    {
    	int ret;
    
    	if (bq24250->pdata->mains_current_limit) {
    		ret = current_to_hw(icl_tbl, ARRAY_SIZE(icl_tbl),
    				    bq24250->pdata->mains_current_limit);
    		if (ret < 0)
    			return ret;
    
    		ret = regmap_update_bits(bq24250->regmap, BQ24250_CONTROL_REG,
    					 BQ24250_IIN_LIMIT, ret);
    		if (ret < 0)
    			return ret;
    	}
    
    	if (bq24250->pdata->usb_hc_current_limit) {
    		ret = current_to_hw(icl_tbl, ARRAY_SIZE(icl_tbl),
    				    bq24250->pdata->usb_hc_current_limit);
    		if (ret < 0)
    			return ret;
    
    		ret = regmap_update_bits(bq24250->regmap, BQ24250_CONTROL_REG,
    					 BQ24250_IIN_LIMIT, ret);
    		if (ret < 0)
    			return ret;
    	}
    
    	return 0;
    }
    
    static int bq24250_set_voltage_limits(struct bq24250_charger *bq24250)
    {
    	int ret;
    
    	if (bq24250->pdata->max_charge_voltage) {
    		ret = bq24250->pdata->max_charge_voltage;
    
    		if (ret < 0)
    			return ret;
    
    		ret = regmap_update_bits(bq24250->regmap,
    					 BQ24250_BATTERY_VOLTAGE_REG,
    					 BQ24250_BATTERY_VOLTAGE, ret);
    		if (ret < 0)
    			return ret;
    	}
    
    	return 0;
    }
    
    static int bq24250_set_ovp_limits(struct bq24250_charger *bq24250)
    {
    	/* Set default - 6V as OVP */
    	return regmap_update_bits(bq24250->regmap,
    				  BQ24250_VOVP_FRC_BATDET_PTM_REG,
    				  BQ24250_VOVP, 0);
    }
    
    static int bq24250_hw_init(struct bq24250_charger *bq24250)
    {
    	int ret;
    
    	/*
    	 * Program the platform specific configuration values to the device
    	 * first.
    	 */
    	ret = bq24250_set_charge_current(bq24250);
    	if (ret < 0)
    		goto fail;
    
    	ret = bq24250_set_current_limits(bq24250);
    	if (ret < 0)
    		goto fail;
    
    	ret = bq24250_set_voltage_limits(bq24250);
    	if (ret < 0)
    		goto fail;
    
    	ret = bq24250_set_ovp_limits(bq24250);
    	if (ret < 0)
    		goto fail;
    
    	ret = bq24250_update_ps_status(bq24250);
    	if (ret < 0)
    		goto fail;
    
    	ret = bq24250_start_stop_charging(bq24250);
    
    fail:
    	return ret;
    }
    
    static irqreturn_t bq24250_interrupt(int irq, void *data)
    {
    	struct bq24250_charger *bq24250 = data;
    	unsigned int irqstat;
    	bool handled = false;
    	int ret;
    
    	dev_info(bq24250->dev, " In %s - Started\n", __func__);
    	ret = regmap_read(bq24250->regmap, BQ24250_STATUS_CONTROL_REG,
    			  &irqstat);
    	if (ret < 0) {
    		dev_warn(bq24250->dev, "reading STATUS_CONTROL_REG failed\n");
    		return IRQ_NONE;
    	}
    
    	irqstat &= BQ24250_FAULT_MASK;
    
    	/*
    	 * If we get charger error we report the error back to user and
    	 * disable charging.
    	 */
    	switch (irqstat)  {
    	case BQ24250_NORMAL:	/* Normal  - No fault */
    		handled = true;
    		break;
    	case BQ24250_INPUT_OVP:	/* Input OVP */
    	case BQ24250_SLEEP:	/* SLEEP */
    	case BQ24250_THERMAL_SHUTDOWN:	/* TS SHUTDOWN */
    	case BQ24250_LDO_SHORT:	/* LDO Short */
    		dev_info(bq24250->dev,
    			"error in charger, disabling charging with \
    			 \"%s\" fault\n", desc[irqstat]);
    		bq24250_vsystem_disable(bq24250);
    		bq24250_charging_disable(bq24250);
    		bq24250_timer_suspend(bq24250);
    		power_supply_changed(&bq24250->battery);
    		handled = true;
    		break;
    	case BQ24250_INPUT_UVLO:	/* Input UVLO */
    		/* If we got an under voltage interrupt it means that
    		    AC/USB input was connected or disconnected.  */
    		dev_info(bq24250->dev,
    			"error in charger, disabling charging with \
    			 \"%s\" fault\n", desc[irqstat]);
    		bq24250_vsystem_disable(bq24250);
    		bq24250_charging_disable(bq24250);
    		bq24250_timer_reset(bq24250);
    		if (bq24250->pdata->use_mains)
    			power_supply_changed(&bq24250->mains);
    		if (bq24250->pdata->use_usb)
    			power_supply_changed(&bq24250->usb);
    		handled = true;
    		break;
    	case BQ24250_BATTERY_TS_FAULT:	/* BAT TS FAULT */
    		dev_info(bq24250->dev,
    			"error in charger, disabling charging with \
    			 \"%s\" fault\n", desc[irqstat]);
    		bq24250_vsystem_enable(bq24250);
    		bq24250_charging_disable(bq24250);
    		bq24250_timer_suspend(bq24250);
    		if (bq24250->pdata->use_mains)
    			power_supply_changed(&bq24250->mains);
    		if (bq24250->pdata->use_usb)
    			power_supply_changed(&bq24250->usb);
    		handled = true;
    		break;
    	case BQ24250_BATTERY_OVP:	/* BAT OVP */
    		dev_info(bq24250->dev,
    			"error in charger, disabling charging with \
    			 \"%s\" fault\n", desc[irqstat]);
    		bq24250_vsystem_disable(bq24250);
    		bq24250_charging_disable(bq24250);
    		bq24250_timer_suspend(bq24250);
    		if (bq24250->pdata->use_mains)
    			power_supply_changed(&bq24250->mains);
    		if (bq24250->pdata->use_usb)
    			power_supply_changed(&bq24250->usb);
    		handled = true;
    		break;
    	case BQ24250_TIMER_FAULT:	/* Timer Fault */
    		dev_info(bq24250->dev,
    			"error in charger, disabling charging with \
    			 \"%s\" fault\n", desc[irqstat]);
    		bq24250_vsystem_enable(bq24250);
    		bq24250_charging_disable(bq24250);
    		bq24250_timer_reset(bq24250);
    		handled = true;
    		break;
    	case BQ24250_NO_BATTERY_CONNECTED:	/* No BAT Connected */
    	case BQ24250_ISET_SHORT:	/* ISET Short */
    		dev_info(bq24250->dev,
    			"error in charger, disabling charging with \
    			 \"%s\" fault\n", desc[irqstat]);
    		bq24250_vsystem_enable(bq24250);
    		bq24250_charging_disable(bq24250);
    		bq24250_timer_suspend(bq24250);
    		if (bq24250->pdata->use_mains)
    			power_supply_changed(&bq24250->mains);
    		if (bq24250->pdata->use_usb)
    			power_supply_changed(&bq24250->usb);
    		handled = true;
    		break;
    	default:
    		dev_err(bq24250->dev,
    			"Charger Fault, disabling charging with \"%s\" unknown fault\n", desc[irqstat]);
    		handled = false;
    		break;
    	}
    
    	return handled ? IRQ_HANDLED : IRQ_NONE;
    }
    
    static int bq24250_irq_set(struct bq24250_charger *bq24250, bool enable)
    {
    	int ret;
    
    	/*
    	* Enable/disable interrupts for:
    	*      - status chage using the STAT pin
    	*      - charger fault error usign the INT pin
    	*/
    	ret = regmap_update_bits(bq24250->regmap, BQ24250_STATUS_CONTROL_REG,
    				 BQ24250_FAULT, enable ? BQ24250_FAULT : 0);
    	if (ret < 0)
    		goto fail;
    
    	ret = regmap_update_bits(bq24250->regmap, BQ24250_CONTROL_REG,
    				 BQ24250_EN_STAT, enable ? 1 : 0);
    
    	if (ret < 0)
    		goto fail;
    
    fail:
    	return ret;
    }
    
    static inline int bq24250_irq_enable(struct bq24250_charger *bq24250)
    {
    	return bq24250_irq_set(bq24250, true);
    }
    
    static inline int bq24250_irq_disable(struct bq24250_charger *bq24250)
    {
    	return bq24250_irq_set(bq24250, false);
    }
    
    static int bq24250_irq_init(struct bq24250_charger *bq24250, int irq)
    {
    	int ret;
    
    	if (irq <= 0) {
    		dev_info(bq24250->dev, "invalid irq number: %d\n", irq);
    		goto out;
    	}
    
    	/*
    	* Configure the STAT output to be suitable for interrupts: disable
    	* all other output (except interrupts) and make it active low.
    	*/
    	regmap_update_bits(bq24250->regmap, BQ24250_STATUS_CONTROL_REG,
    			   BQ24250_EN_STAT, 1);
    
    	ret = request_threaded_irq(irq, NULL, bq24250_interrupt,
    				   IRQF_TRIGGER_RISING | IRQF_ONESHOT,
    				   "bq24250_irq", bq24250);
    	if (ret)
    		return ret;
    
    	bq24250->irq = irq;
    	bq24250_irq_enable(bq24250);
    out:
    	return 0;
    }
    
    static ssize_t bq24250_show_charger_fault(struct device *dev,
    					  struct device_attribute *attr,
    					  char *buf)
    {
    	unsigned int val;
    	int ret;
    	struct bq24250_charger *bq24250 = dev_get_drvdata(dev);
    
    	ret = regmap_read(bq24250->regmap, BQ24250_STATUS_CONTROL_REG, &val);
    	if (ret < 0)
    		return 0;
    
    	val &= BQ24250_FAULT_MASK;
    
    	return scnprintf(buf, PAGE_SIZE, "%s\n", desc[val]);
    }
    
    static DEVICE_ATTR(charger_fault, S_IRUSR, bq24250_show_charger_fault, NULL);
    
    static struct attribute *bq24250_charger_attr[] = {
    	&dev_attr_charger_fault.attr,
    	NULL,
    };
    
    static const struct attribute_group bq24250_attr_group = {
    	.attrs = bq24250_charger_attr,
    };
    
    
    /*
     * Returns the constant charge current programmed
     * into the charger in mA.
     */
    static int get_const_charge_current(struct bq24250_charger *bq24250)
    {
    	int ret;
    	unsigned int val, intval;
    
    	if (!bq24250_is_ps_online(bq24250))
    		return -ENODATA;
    
    	ret = regmap_read(bq24250->regmap, BQ24250_TERM_CURR_CHARG_REG, &val);
    	if (ret < 0)
    		return ret;
    
    	val >>= BQ24250_CHARGE_CURR_SHIFT;
    	val &= BQ24250_CHARGE_CURR;
    
    	intval = hw_to_current(cc_tbl, ARRAY_SIZE(cc_tbl), val);
    
    	if (intval == 0)
    		intval = 0xf;
    	else
    		intval = 500 + val * 50;
    
    
    	dev_info(bq24250->dev, "const charge current is %d mA\n", intval);
    	return intval;
    }
    
    /*
     * Returns the constant charge voltage programmed
     * into the charger in mV.
     */
    static int get_const_charge_voltage(struct bq24250_charger *bq24250)
    {
    	int ret;
    	unsigned int val;
    	int intval;
    
    	if (!bq24250_is_ps_online(bq24250))
    		return -ENODATA;
    
    	ret = regmap_read(bq24250->regmap, BQ24250_BATTERY_VOLTAGE_REG, &val);
    	if (ret < 0)
    		return ret;
    
    	val >>= BQ24250_BATTERY_VOLTAGE_SHIFT;
    	val &= BQ24250_BATTERY_VOLTAGE;
    
    	if (val > 0x30)
    		val = 0x30;
    
    	intval = hw_to_current(brv_tbl, ARRAY_SIZE(brv_tbl), val);
    
    	/* intval = (3500 + val)/1000; */
    	intval += 3500;
    	dev_info(bq24250->dev, "const charge voltage is=%d mV\n", intval);
    	intval = 3500 + val * 20;
    	dev_info(bq24250->dev, "const charge voltage is=%d mV\n", intval);
    
    	return intval;
    }
    
    static int bq24250_mains_get_property(struct power_supply *psy,
    				     enum power_supply_property prop,
    				     union power_supply_propval *val)
    {
    	struct bq24250_charger *bq24250 =
    		container_of(psy, struct bq24250_charger, mains);
    	int ret;
    
    	switch (prop) {
    	case POWER_SUPPLY_PROP_ONLINE:
    		val->intval = bq24250->mains_online;
    		break;
    
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE:
    		ret = get_const_charge_voltage(bq24250);
    		if (ret < 0)
    			return ret;
    		else
    			val->intval = ret;
    		break;
    
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT:
    		ret = get_const_charge_current(bq24250);
    		if (ret < 0)
    			return ret;
    		else
    			val->intval = ret;
    		break;
    
    	default:
    		return -EINVAL;
    	}
    
    	return 0;
    }
    
    static int bq24250_usb_get_property(struct power_supply *psy,
    				   enum power_supply_property prop,
    				   union power_supply_propval *val)
    {
    	struct bq24250_charger *bq24250 =
    		container_of(psy, struct bq24250_charger, usb);
    	int ret;
    
    	switch (prop) {
    	case POWER_SUPPLY_PROP_ONLINE:
    		val->intval = bq24250->usb_online;
    		break;
    
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_VOLTAGE:
    		ret = get_const_charge_voltage(bq24250);
    		if (ret < 0)
    			return ret;
    		else
    			val->intval = ret;
    		break;
    
    	case POWER_SUPPLY_PROP_CONSTANT_CHARGE_CURRENT:
    		ret = get_const_charge_current(bq24250);
    		if (ret < 0)
    			return ret;
    		else
    			val->intval = ret;
    		break;
    
    	default:
    		return -EINVAL;
    	}
    
    	bq24250_update_usb_type(bq24250);
    
    	return 0;
    }
    
    static int bq24250_battery_get_property(struct power_supply *psy,
    				       enum power_supply_property prop,
    				       union power_supply_propval *val)
    {
    	struct bq24250_charger *bq24250 =
    			container_of(psy, struct bq24250_charger, battery);
    	const struct bq24250_charger_platform_data *pdata = bq24250->pdata;
    	int ret;
    
    	ret = bq24250_update_ps_status(bq24250);
    	if (ret < 0)
    		return ret;
    
    	switch (prop) {
    	case POWER_SUPPLY_PROP_STATUS:
    		if (!bq24250_is_ps_online(bq24250)) {
    			val->intval = POWER_SUPPLY_STATUS_DISCHARGING;
    			break;
    		}
    
    		switch (bq24250_charging_status(bq24250)) {
    		case 0:
    			val->intval = POWER_SUPPLY_STATUS_DISCHARGING;
    			break;
    		case 1:
    			val->intval = POWER_SUPPLY_STATUS_CHARGING;
    			break;
    		case 2:
    			val->intval = POWER_SUPPLY_STATUS_FULL;
    			break;
    		case 3:
    			val->intval = POWER_SUPPLY_STATUS_UNKNOWN; /* FAULT */
    			break;
    		}
    		break;
    
    	case POWER_SUPPLY_PROP_CHARGE_TYPE:
    		if (!bq24250_is_ps_online(bq24250))
    			return -ENODATA;
    
    		/*
    		 * We handle trickle and pre-charging the same, and taper
    		 * and none the same.
    		 */
    		switch (bq24250_charging_status(bq24250)) {
    		case 1:
    			val->intval = POWER_SUPPLY_CHARGE_TYPE_TRICKLE;
    			break;
    		case 2:
    			val->intval = POWER_SUPPLY_CHARGE_TYPE_FAST;
    			break;
    		default:
    			val->intval = POWER_SUPPLY_CHARGE_TYPE_NONE;
    			break;
    		}
    		break;
    
    	case POWER_SUPPLY_PROP_TECHNOLOGY:
    		val->intval = pdata->battery_info.technology;
    		break;
    
    	case POWER_SUPPLY_PROP_VOLTAGE_MIN_DESIGN:
    		val->intval = pdata->battery_info.voltage_min_design;
    		break;
    
    	case POWER_SUPPLY_PROP_VOLTAGE_MAX_DESIGN:
    		val->intval = pdata->battery_info.voltage_max_design;
    		break;
    
    	case POWER_SUPPLY_PROP_CHARGE_FULL_DESIGN:
    		val->intval = pdata->battery_info.charge_full_design;
    		break;
    
    	case POWER_SUPPLY_PROP_MODEL_NAME:
    		val->strval = pdata->battery_info.name;
    		break;
    
    	default:
    		return -EINVAL;
    	}
    
    	return 0;
    }
    
    static enum power_supply_property bq24250_battery_properties[] = {
    	POWER_SUPPLY_PROP_STATUS,
    	POWER_SUPPLY_PROP_CHARGE_TYPE,
    	POWER_SUPPLY_PROP_TECHNOLOGY,
    	POWER_SUPPLY_PROP_VOLTAGE_MIN_DESIGN,
    	POWER_SUPPLY_PROP_VOLTAGE_MAX_DESIGN,
    	POWER_SUPPLY_PROP_CHARGE_FULL_DESIGN,
    	POWER_SUPPLY_PROP_MODEL_NAME,
    };
    
    static int bq24250_power_supply_register(struct bq24250_charger *bq24250)
    {
    	static char *battery[] = { "bq24250-battery" };
    	int ret;
    
    	if (bq24250->pdata->use_mains) {
    		bq24250->mains.name = "bq24250-mains";
    		bq24250->mains.type = POWER_SUPPLY_TYPE_MAINS;
    		bq24250->mains.get_property = bq24250_mains_get_property;
    		bq24250->mains.properties = bq24250_charger_properties;
    		bq24250->mains.num_properties =
    					ARRAY_SIZE(bq24250_charger_properties);
    		bq24250->mains.supplied_to = battery;
    		bq24250->mains.num_supplicants = ARRAY_SIZE(battery);
    
    		ret = power_supply_register(bq24250->dev, &bq24250->mains);
    		if (ret < 0)
    			return ret;
    	}
    
    	if (bq24250->pdata->use_usb) {
    		bq24250->usb.name = "bq24250-usb";
    		bq24250->usb.type = POWER_SUPPLY_TYPE_USB;
    		bq24250->usb.get_property = bq24250_usb_get_property;
    		bq24250->usb.properties = bq24250_charger_properties;
    		bq24250->usb.num_properties =
    					ARRAY_SIZE(bq24250_charger_properties);
    		bq24250->usb.supplied_to = battery;
    		bq24250->usb.num_supplicants = ARRAY_SIZE(battery);
    
    		ret = power_supply_register(bq24250->dev, &bq24250->usb);
    		if (ret < 0) {
    			if (bq24250->pdata->use_mains)
    				power_supply_unregister(&bq24250->mains);
    			return ret;
    		}
    	}
    
    	bq24250->battery.name = "bq24250-battery";
    	bq24250->battery.type = POWER_SUPPLY_TYPE_BATTERY;
    	bq24250->battery.get_property = bq24250_battery_get_property;
    	bq24250->battery.properties = bq24250_battery_properties;
    	bq24250->battery.num_properties =
    				ARRAY_SIZE(bq24250_battery_properties);
    
    	ret = power_supply_register(bq24250->dev, &bq24250->battery);
    	if (ret < 0) {
    		if (bq24250->pdata->use_usb)
    			power_supply_unregister(&bq24250->usb);
    		if (bq24250->pdata->use_mains)
    			power_supply_unregister(&bq24250->mains);
    		return ret;
    	}
    
    	return 0;
    }
    
    static void bq24250_power_supply_unregister(struct bq24250_charger *bq24250)
    {
    	power_supply_unregister(&bq24250->battery);
    	if (bq24250->pdata->use_usb)
    		power_supply_unregister(&bq24250->usb);
    	if (bq24250->pdata->use_mains)
    		power_supply_unregister(&bq24250->mains);
    }
    
    static const struct regmap_config bq24250_regmap = {
    	.reg_bits         = 8,
    	.val_bits         = 8,
    
    	.max_register     = BQ24250_MAX_REGISTER,
    	.reg_defaults     = bq24250_reg_defs,
    	.num_reg_defaults = ARRAY_SIZE(bq24250_reg_defs),
    	.cache_type	  = REGCACHE_RBTREE,
    };
    
    static int bq24250_probe(struct i2c_client *client,
    			const struct i2c_device_id *id)
    {
    	const struct bq24250_charger_platform_data *pdata;
    	struct device *dev = &client->dev;
    	struct bq24250_charger *bq24250;
    	int ret;
    
    	pdata = dev->platform_data;
    	if (!pdata) {
    		printk(KERN_NOTICE "In probe - failed with NO PDATA\n");
    		return -EINVAL;
    	}
    
    	bq24250 = devm_kzalloc(dev, sizeof(*bq24250), GFP_KERNEL);
    	if (!bq24250)
    		return -ENOMEM;
    
    	bq24250->dev = &client->dev;
    	bq24250->pdata = client->dev.platform_data;
    	i2c_set_clientdata(client, bq24250);
    
    	bq24250->regmap = devm_regmap_init_i2c(client, &bq24250_regmap);
    	if (IS_ERR(bq24250->regmap))
    		return PTR_ERR(bq24250->regmap);
    
    
    	ret = bq24250_hw_init(bq24250);
    	if (ret < 0) {
    		dev_err(dev, "failed to initialize BQ24250 chip: %d\n", ret);
    		goto err_dev;
    	}
    
    	ret = bq24250_power_supply_register(bq24250);
    	if (ret < 0) {
    		dev_err(dev, "failed to register power supply: %d\n", ret);
    		goto err_dev;
    	}
    
    	ret = sysfs_create_group(&dev->kobj, &bq24250_attr_group);
    	if (ret < 0) {
    		dev_err(dev, "failed to add charge sysfs: %d\n", ret);
    		goto err_sysfs;
    	}
    
    	/*
    	 * Interrupt pin is optional. If it is connected, we setup the
    	 * interrupt support here.
    	 */
    	ret = bq24250_irq_init(bq24250, client->irq);
    	if (ret < 0) {
    		dev_warn(dev, "failed to initialize IRQ: %d\n", ret);
    		dev_warn(dev, "disabling IRQ support\n");
    	}
    
    	return 0;
    
    err_sysfs:
    	bq24250_power_supply_unregister(bq24250);
    err_dev:
    	return ret;
    }
    
    static int bq24250_remove(struct i2c_client *client)
    {
    	struct bq24250_charger *bq24250 = i2c_get_clientdata(client);
    
    	if (bq24250->irq) {
    		bq24250_irq_disable(bq24250);
    		free_irq(bq24250->irq, bq24250);
    	}
    
    	sysfs_remove_group(&bq24250->dev->kobj, &bq24250_attr_group);
    	bq24250_power_supply_unregister(bq24250);
    
    	return 0;
    }
    
    static const struct i2c_device_id bq24250_id[] = {
    	{ "bq24250", 0 },
    	{ }
    };
    MODULE_DEVICE_TABLE(i2c, bq24250_id);
    
    static struct i2c_driver bq24250_driver = {
    	.driver = {
    		.name = "bq24250",
    		.owner = THIS_MODULE,
    	},
    	.probe        = bq24250_probe,
    	.remove       = __devexit_p(bq24250_remove),
    	.id_table     = bq24250_id,
    };
    
    module_i2c_driver(bq24250_driver);
    
    MODULE_DESCRIPTION("BQ24250 battery charger driver");
    MODULE_AUTHOR("MR Swami Reddy <mr.swami.reddy@ti.com>");
    MODULE_LICENSE("GPL v2");
    

  • Please see attached example c code. Keep in mind that the charger only has internal registers to which you read and write. It does not a processor.
  • Very nice, thanks. I suppose that I should have specified that I was looking for a .Net micro framework driver. This is Linux, correct? It should be helpful anyway. Would you happen to also have something similar for a gas gauge such as the BQ27421?