This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Li-ion cell ; +5V & 1.5A output

Genius 3300 points
Other Parts Discussed in Thread: TPS81256, TPS61230

1. I have multiple li-ion cell in parallel, combined output voltage varies: 3.3V to 4.2V.

2. I need to get +5V from it at 1.5A current.

3. is there any solution for it?

4. Can I connect multiple TPS81256 in parallel to increase the current range?