A few questions related to the use of the part.
- Is there any difference in the behavior of the part in the following two configurations? Is one mode preferred?
- ISET = 540R, ISET2 = High
- ISET = 540/.462 = 1.17K, ISET2 = Low
- If strapping ISET2 high/low, is it preferable to use a resistive connection or direct connection?
- If using the USB500 mode, is Pre-Term value referenced to the ISET strap, or is it based on the 462mA (typ) of the USB500 setting?
Thank you for your time.
Mike