I have a 20V source that I am regulating down to 12V using LM2679T-12. Initially, the regulator was soldered to the board and testing was carried out to drive 2 linear actuators. When the regulator was soldered to the board, the regulator was able to drive 2 linear actuators. However, for my project, the regulator needs to be mounted away from the board. Therefore, wires are soldered to the pins of the regulator and are connected to the board.
When the wires are short (less than 3"), the regulator still works fine. On the other hand, when we use longer wires (we need the wires lengths to be at least 6"), problems start appearing: the output of the regulator initially starts at 12V. However, when the actuator is activated the voltage drops below 4V and the actuator does not move any more.
I was wondering if anyone might know what I am missing. Do the lengths of the wires affect the output voltage because of the switching? Is this something that could be compensated for using different values for the LC filter?
I can supply more information if needed.
Thank you in advance for your help.