The LM5030 list a shutdown threshold to be within the range of 0.2V to 0.7V. However, the first gate drive pulse is seen when the softstart pin reaches 1.05V. This was seen on three separate chips to verify that the measurement was correct. Is there a turn-on threshold that is different than the shutdown threshold? If so, what is it, and is it guaranteed over the part’s entire temperature range.