This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210 output variation 100V Ok 50V needed

Other Parts Discussed in Thread: TINA-TI

hi,
I have done circuit for 100 Vdc with 12 V input. now i have a doubt
1. is it possible to get 50V with same circuit. if yes what should i do weather introduce voltage divider into the output Or need to make change in switching function
2. I have tried with voltage divider in simulation i am getting exactly 50 V as a output but when we introduce voltage divider for high voltage circuit produce high heat. so what is possibility to get 50 V.
3. if need to change in switching circuit how to do that.