Hello,
I have been asked to provide an isolated dc-dc converter with the following charactaristics:
Input: Nominal 24 VDC
Outputs: dual +/- 12 VDC
Output power: <100mA
What TI units would fit this application?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have been asked to provide an isolated dc-dc converter with the following charactaristics:
Input: Nominal 24 VDC
Outputs: dual +/- 12 VDC
Output power: <100mA
What TI units would fit this application?
Thanks
Do you in fact need an isolated solution?
Hi John,
What we are hoping to source is a 24Vinput converter with 2 X 12V output hooked together with a center 0V (ground). This is powering a mobile audio application where a dual power supply is required.12V+, 0V ground, 12V-.
Since this is an audio application we are concerned about keeping noise out of the amplifier stage. Perhaps unduly so.
Thanks for your interest.
Hal