Hi friend, i am junior in switch power.
Now, i am use UCC28251 to design full-bridge power, the followings are the parameter:
input voltage: 200Vdc-320Vdc
output : 28V/46A
switch frequency is 100KHz
Transformer: Np=13Ts, Ns=4Ts,L=800uH, the core is EE55
filter inductance: L=20uH
i have some questions:
1st. There is a separate power to supply UCC28251, first, the aux power is switch on, and the D=50%; then the input power is switch on, the UCC28251 soft-start is just 20ms, after 20ms, the IC is switch off. i am really do not know why it is off. i check the datasheet, there are four reason that the IC could off, first VDD undervoltage; 2nd is EN undervoltage; 3rd is OVP; 4th is over temperature. But I think my circuit is not the above reason.
2nd. it is the same as 1st. first the input voltage is switch on, then the aux power is one. but the UCC28251 was notwork at all.
i am really hopeful that u can reply my questions. i am looking for your answer
best regard