Hi there,
I designed 4-layer PCB that contains a single cell battery charger BQ24195 and is controlled by I2C commands, so I'm able to set up into boost mode operation from battery, getting a PMID output voltage of 5.1V.
However, on the scenario of IPMID = 0, the battery is discharged at rate of 15mA (typ) as stated on the datasheet:
I notice that in boost mode, REGN LDO is still ON (~5V) when the input is removed and therefore BQ24195 isn't in high impedance ... I tried to set to REG00[7] = 1, but then boost mode is disabled.
Since my board is mainly to be used as power bank (in boost mode), I wonder is there a way to decrease the constant battery discharge current when no device is connected to the PMID output?
Thank you in advance!
Regards,
Carlos.