This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Calculate external emulated ripple injection for LM3150

Other Parts Discussed in Thread: LM3150

Hi All,

I'm trying to calculate external emulated ripple injection circuit for LM3150.

I can't find the minimum peak to peak ripple voltage for the FB pin in the datasheet of LM3150, can you pleas suggest me where to look for the information.

My specification for the power supply:

Vout=5V

Vin_min= 7V

Vin_max= 24V

Max load current =5A

Typ. load current 3A

Soft start =1.1ms

fs= 250kHz

D=0.417

I tried to calculate the elements for the ripple injection circuit for my case with 30mV p-p ripple

And here are the values:

Rr=250kOhm

Cr= 510pF

Cac= from 1600pF to 2000pF

Is there some documentation how to calculate this?

Thank for any suggestion and help.

Best Regards,

David.