Hi all,
I'm new in this devices and I want to ask some questions.
I've seen that BQ24075 have 2 usb modes(100mA and 500mA) and a wall adapter mode.
- There is a way to create a general mode that is good for USB and Wall adapter?
I explain better, If I set more than 500mA like 700mA, 1A or 1.5A and connect it to a PC-USB port, It can damage it?
- Can BQ24075 power my circuitry when is usb connected? Even if battery is discharged or disconnected?
- In datasheed is explained that BQ24075 signal when battery is fully charged. Can it also indicate battery charge status? Also, can it indicate battery status when is USB unplugged and powered on(when circuit is powered)?
- If the last question answer is negative, there is possibility to integrate a gas gauge to measure charging status during charge and battery charge status during power on? Or there is already a build in device that have BQ24075 and gas gauge functionality?
Thank you.