Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118 Output Issue

Other Parts Discussed in Thread: LM5118

Dear all.

Our customer has caused trouble.
When LM5118 is Buck/Boost mode and the voltage of input and output is near voltage and hangs a load, a BOOST circuit doesn't function.
This is in the state like Figure 9 between 15V and 16V.
Even if input/output is changed to BUCK mode state, BOOST doesn't work.
ex. output setting=10V ->8V (because BOOST does't work)
The FB voltage is also 1.18V at the same time.
Their circuit is as following;

Could you send your comment to me?