I am testing battery chargin with the EVM, I replaced the current sense resistor (R6) as well as R13/R15 for charge current. I have other EVMs that have the same replacements that are verfified working, but for this EVM it is not charging.
When powered from a DC supply to charge a Li-ion battery pack, nothing happens. As soon as I disconnect the positive battery lead, STAT1 lights up to indicate it is charging, but that is not the case as the battery is disconnected. When the battery lead is connected STAT1 turns off and no charge is applied to the battery.
Ideas as to why STAT1 would be pulled low with no battery connected?