Design scenario: A 3.3V battery is wired to Vin of the regulator, with an output voltage set a little higher (e.g. 4V), approximately 1uH inductor in use, and about 100uF capacitance present on Vin and Vout. Vout is wired directly to the load
A slightly higher (e.g. 4.2V) voltage source or power supply will for some of the time be wired directly to Vout and the load. According to the datasheet, section 8.4.3 "Zero Duty Cycle Mode" :
When the input voltage is lower than VOUT + 0.24 V and VOUT is higher than the nominal output voltage, the device automatically changes to a Zero Duty Cycle Mode. In Zero Duty Cycle Mode, the rectifying switch is constantly turned on and the low side switch is turned off.
This will result in the rectifying switch being constantly turned on, and thus Vout being connected directly to the battery in this case, resulting in massive current and possible failure of the battery and/or device. Is this correct or is the datasheet in error ?