Hi Everyone,
Please let me ask about Ron of internal Q1 FET of bq24308. The VDO at 250mA is specified as 75mV max, so I understand that the Ron max at 250mA should be 300mohm. Then is it also the same at 1.5A ? If so, it looks large because the dropout will be 0.45V at 300mohm and 1.5A.
It will be helpful if you can provide the characteristics of VDO vs IOUT.
Best Regards,
Sonoki / Japan Disty