HELLO.
I have a question about TPS3700.
Condition
Vdd=0V(Not Power)
Ina+,Ina-=5V (add Voltege)
Would IC receive damage at the same time?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HELLO.
I have a question about TPS3700.
Condition
Vdd=0V(Not Power)
Ina+,Ina-=5V (add Voltege)
Would IC receive damage at the same time?
Thank you.
Hi Ishii-san,
If 5V is applied to either INA or INB, and VCC is connected to GND or if it has a lot of capacitance, then yes the IC can be damaged.Inside our ESD diodes would conduct current from INA to VCC and if there is no resistance, then the current may damage the ESD structures.
So now my questions:
1. Why would 5V be added to INA or INB as these are 400mV thresholds?
2. Do you have resistors in the above scenario or or you looking at a worst case condition?
Regards,