This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Inverting Charge Pump IC for -100V Output

Other Parts Discussed in Thread: TPS40210

Hi

I have made a DC-DC converter circuit using TPS40210 to get 100 V with 100 mA output. Am using this to power an op-amp.

My op-amp is being used as a square wave generator which is driving a piezoelectric device. In this circuit my +Vsat is 100V and -Vsat is GND.

I need to provide a -Vsat of -100V. To do this i planned on inverting the 100V DC-DC converter output.

While searching the internet i came across inverting charge pump/ switching capacitor voltage converter ICs. The ICs I found can provide an output of -32V only.

Can you please suggest an IC which meets the said requirement.