This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PANTHER_BOARD_DM3730_BOOTING_ISSUE

Other Parts Discussed in Thread: TPS65950, DM3730

Hi,

I am using Panther board (JORJIN AP Module ATBN441JS (DM3730 +TPS65950) with OS Ubuntu12.10,kernel version 3.7.10).We are Booting board using SD card.Sometimes it boots perfectly ,Sometimes  SD card stuck with errors at different positions or kernel panic happens,But the same sd card works fine on another board with same AP module .

 

Is it related with ram size or DDR frequency in u-boot?

Also I need to check memory size from u-boot,I tried MTEST command from u-boot But it stuck with 

Testing.......

Iteration 1

How I test memory using MTEST command?

Can Anyone help me to solve this problem??