Hello,
I am interested in using the UCD3138 for a design.
To learn the device, I have downloaded the training labs from this website.
However, I have not been able to compile the labs, even after using the project file converter in the GUI and setting the processor options to 32 bit.
Here is a screenshot of the errors I get when I try to build:
Here is a screenshot of my general build options:
I noticed that the training lab files were made with CCS3.3.
Is there a ‘correct’ version of CCS I need to use for the UCD3138?
Is it even possible to use CCS6.1?
Thanks