I only want to use this as an “Ideal Diode” with load switching and do not want any of the other protection functions.
I see how the under and over voltage functions can be disabled, but am wondering if it is possible to disable to current sense feature as well.
I also do not want to slow down the switching time of the FET with the “Timer” pin. I am assuming I can just leave this floating to ensure the FET will respond as fast as possible?