Hi!
I need to convert a single 5Vdc supply into +5V and -5V for sensor buffer amplifiers. Due to the number of amplifiers, around 500mA of current is needed. I found the TPS65133 and I like the fact that it requires only a few external parts.To get to the desired current, two of these chips would have to be placed in parallel. Is this possible or will it cause problems?
Best regards,
Wouter