Hello,
we are using the TPS65132W in a new project to generate +-5.4V.
Unfortunatly, after building up the board, we're measuring +4V and -4V on the output rails instead of the expectet 5.4V. Is there a possible explanation why the controller sets this minimum values? ENP, ENN, SDA and SCL are tied up to the input voltage (5V) by small resistors.
Thank You for