Hi all,
I am quite new in this area and I have a couple of questions.
1) Do you know how do you choose the gate resistance for a MOSFET when the Texas instruments UCC27211DDA gate driver is used? I am using the MOSFET (150V, 100A) as per table below, in my design for a dc-dc converter. The mosfet gate will be connected (via the external resistance whose value I need to choose), to the gate driver PIN HO. Also, the MOSFET switching frequency will be 200kHz.
2) what is the voltage coming out of the UCC27211 pin HO? (this will be the PIN connected to the gate driver via the external resistor)
PS below is the MOSFET data:
Datasheets |
|
---|---|
Product Photos |
|
Family |
|
FET Type |
MOSFET N-Channel, Metal Oxide |
FET Feature |
Standard |
Drain to Source Voltage (Vdss) |
150V |
Current - Continuous Drain (Id) @ 25°C |
100A (Tc) |
Rds On (Max) @ Id, Vgs |
7.2 mOhm @ 100A, 10V |
Vgs(th) (Max) @ Id |
4V @ 270µA |
Gate Charge (Qg) @ Vgs |
93nC @ 10V |
Input Capacitance (Ciss) @ Vds |
5470pF @ 75V |
Power - Max |
300W |
Thank you so much,
Leonardo