This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC9081 I2C issue

Other Parts Discussed in Thread: UCD9081

Hi,

We are using UCD9081 in our board. Every time we connect the board to GUI it detects random I2C address. Two of the address pins are left floating. Is this causing the address to change randomly?

Regards

Madhura

  • Yes. 

    The UCD9081 selects an I2C address by sampling the logic level of the four digital inputs to the device (ADDR1–ADDR4) during the RESET interval. When the UCD9081 is released from RESET, the ADDRx logic levels are latched and the I2C address is assigned. External pullup/pulldown resistors are required to configure the I2C address; the UCD9081 does not have internal bias resistors.