This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

charger requirement

Guru 29720 points
Other Parts Discussed in Thread: BQ24075

Hi Team,

My customer is looking for charger device for wearable application.
The requirement is the following.
--------------------------------------------------------
1) battery: 1 cell Li-ion
2) Power Path
3) input voltage: 5V
4) standalone
5) battery charge voltage: adjustable (programmable using external resistors etc..)
6) battery charge current: 0.5~1.5A
--------------------------------------------------------
Is there any TI device that meets the requirement?
Especially, I would like to know the device that meets both 4 and 5.
The background of requirement of 5 is my customer considers to use this charger for several varieties models the battery voltage of these are 4.2V and 4.35V.
He doesn't want host control(I2C) device.

Yaita / Japan disty