This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61236 application question

Dear Sir

we want use TPS61236 in Vin 3.2~5V/ Vout 5V /3A application. 

may we check if TPS61236 have 100% Duty-Cycle Mode when VIN > VOUT?

or if there have any risk that Vin=Vout =5V?

                                          Best regards,

                                                            Bogey

  • HI Bogey

    this device can't support VIN=VOUT, the VIN must be 0.6V lower than VOUT

    may i know why there is 5V in the VIN?

    thanks
    Jasper Li
  • Hi Jasper

    it is due to customer have 2 power source battery in and DC in.

                                     Best regsrds,

                                                    Bogey

  • hi Bogey

    i guess the battery voltage is 3.3~4.2 V and DC voltage is 5 V from USB. What about bypass the 5V input directly to the VOUT of the TPS61236 using an external mosfet? So the device don't need to operate at VIN=VOUT condition.

    may i know more about the application

    1. how customer separate the two input power: battery and 5-V DC .

    2. what is the end product and what TPS61236 is used to power?

    Thanks

    Jasper Li