I am using the TPS7A49 and cannot shut down the regulator even when the EN pin is directly connected to ground.
The same topology being used is the same as suggested in the data sheet along with the suggested values for all of the capacitors.
Operating Parameters:
Vin = 3.3-5.5V
Vout = 3.0V
Iout < 0.075mA
Component Values:
Vin = 3.3-5.5V
R1 = 124k
R2 = 80.6k
CIN = 10uF, X7R, 0603
COUT = 10uF, X7R, 0603
CNR/SS = 10nF, X7R, 0603
CFF = 10nF, X7R, 0603
Does anyone have any ideas?
Thanks in advance for your help.