What is the best boost converter to recommend with the following specs and cost then size being a concern?
Vin: 3.7V
Vout: 5V
Iout: 500mA
Size and cost are the main drivers.
Current suggestion was TPS61046.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS61256 will offer a smaller solution, since the switching frequency is three times faster. I ran a webench simulation and the solution size is 43 mm^2. The 1 ku price of the TPS61256 is just a little higher than the TPS61046.