This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

replacement for TPS7A4700 and TPS7A3301? what about LM2576?

Other Parts Discussed in Thread: LM2576

Hi, we do not like the QFN package of the TPS7A4700 since we have failed many times. While we can keep using TSP7A3301 since it has a through hole package, we would like to ask whether you have any similar products with easier soldering package to replace TPS7A4700. I find LM2576, but not sure whether it can be used in combination with TPS7A3301 to supply +/- 15V. And I do not find the noise level about this device. What we want are DC/DC regulators where input is +/-(16.5-22 V), output want to be +/-(15-17 V), I out(min)=250 mA, better find something around 1A or 2A. Noise is as low as possible. Hope you can find some chips that are not surface mount or at least not QFN! Thank you!

Best,

Min

  • Hi Min,

    LM2576 is a switching converter rather than an LDO. You will have switching noise with that device.

    Take a look at TPS7A4501. This LDO may be a little easier for you to solder although it is still surface mount.

    Very Respectfully,
    Ryan