This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195 EVM connected to USB SDP port.Input current limit is set to 500mA.Fast charge current to 512mA.Then I found currents across PMID=740mA,VSYS=520mA,BAT=472mA.

Other Parts Discussed in Thread: BQ24195

I have connected 6ohm load across PMID & 6 ohm load across VSYS of BQ24195 EVM and then EVM  to USB port.By default after connecting to USB it is entering into high impedance(HIZ)  state.

Then I wrote

REG00 to 32 to limit input current limit to 500mA &

REG02 to 00 to set fast charge current to 512mA.

Then I found that PMID current =740mA.

VSYS current =520mA

BAT current= 472mA

is it okay  because SDP can source max 500mA.And 500mA not equal to (740+520+472)mA