Will the UCC28063A work for aircraft single and three phase power at 400 Hz. If not, what range of frequencies will it support?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
John,
Thanks for your response. The end application is AC to DC power conversion from 400Hz, 115 AC to DC with control of the harmonics and power factor in the aircraft. I am thinking to utilize both single phase as well as three phase based on the power requirement. Do you have any recommendations for this? The goal is to implement this system without a processor.
Hello James,
I designed a 900 W PFC for the A350 that had to meet the DO 160. I seem to remember that the PF requirement was reasonably low, however the harmonic content specification was very challenging. And this requirement infers a high power factor since power factor is proportional to distortion factor and harmonic content.
Or you can meet the requirement with low active power factor and passive harmonic traps. Our customer did not want that approach since harmonic traps are large and heavy. Weight is very important in aerospace as you know.
The commercial/industrial ICs did not help since the frequency range for aircraft power is from 400 Hz to 800 Hz. The multiplier in the UC3854 is not designed to keep up with this high frequency. We could not reduce the "cusping" that occurs at the zero crossing on the sinewave input. We designed a discrete PFC based on the UC3842 and a wide-bandwidth multiplier IC. I designed this circuit in 2009, We also used a nonlinear ramp and were able to achieve 0.99 PF. There may be ICs available that can work at 800 Hz. I am not sure.
I can provide more assistance off line if you want .
Good luck with your project.
Chuck