Hello,
We have two questions about UVLO in the LM3481 part.
Design info:
R7 = 100K
R8 = 69.8K
Vsh = 3V (calculated)
Ven = 3.5V (calculated)
Hyst = 500mV (calculated)
Additional info:
Fsw = 500Khz
Topology = SEPIC with coupled inductor
Cin = 100uF
Cout = 660uF
Iout = 2A max.
Questions:
1- Maximum hysteresis that can be configured? Could be above 500mV? The UVLO is not working as expected when powered from lithium battery, when the Vin reaches 3V the IC stops switching but quickly returns to normal state. The battery voltage rising is only about 0.35V when the UVLO triggers at 3V.
2- Maximum R7 & R8 values?
Thank you.