A LLC resonant converter must operate above circuit resonance to keep the mosfets switching at zero voltage. In the design suggested in the UCC29950 data sheet, a circuit resonance of 120 kHz was used. The UCC29950 lowers the switching frequency as low as 70 kHz in response to increased load. How does the UCC29950 know when to stop lowering the switching frequency so as to stay above circuit resonance? Other resonant controllers have pins to set the minimum switching frequency, but no such pins exist on the UCC29950.