Hi all,
Our customer requires the device that they can use at the following condition. Do you have any solution?
Vin: 3.1V(min), 3.3V(typ), 3.4V(max)
Vout: -16V
Iout: 60mA
efficiency requirement is 80% over
If you have any solution, please let me know.
Best Regards,
Kohei Sasaki