This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Protecting against reversed Batteries that are in Parallel

Other Parts Discussed in Thread: SM74611

I have a low power application and we have 2 Lithium 3.6V batteries in parallel as well as an external 3.3V input.  I currently use 3 schottky diodes to protect against reversed batteries but the voltage drop of 150mV is too much during certain conditions.  Is there a simpler method i can use that will drop less than 50mV and use no more than 10uA?

Thanks.