I am prototyping with a TPS61202 to see if it will work for a solar application.
I connected a 0.5V 1A source to the input and at no load I got an expected 5V out. Under load I was only getting about 12mA out. I doubled the voltage input to 1V with the same 1A input and the output current dropped to 4.7mA.
Based on Figure 1 in the datasheet, I expected this to increase the current out, not decrease it.
I am using a 2.2uH inductor.
Any thoughts on what I may be doing wrong in my design?
Also, is there any chance I can get on the phone with someone about this? I have not had a great track record with online forms.
Thanks,