HI,
I 'm using on TPS54260 for supply for the GSM module in automotive purpose, following are the input and output details
WHAT IS THE COMPONENTS VALUE FOR THE COPMPENSATION ZERO ( REISITOR VALUE AND CAPACITOR VALUE) AND COMPENSATION POLE
input volt is 24 volt
output is 5 volt
peak current is 2 A
Iinductor L1 is 10uH
out put filtering capcitor is 100uf
swtiching frequency is 300 khz