I have posted my question in the wrong forum initially. I was redirected to this forum. Hopefully someone from here can also expand on the answers I got from my other post.
My question involves several design issues/inquiries in low-powered sensing applications. I would like an opinion or an advice on the matter. First, my project involves:
- A microcontroller
- Sensors
- RF Modules
My aim is to regulate/control the power into each of the devices independently (i.e. Sensors and RF). These components share the same voltage line which is supplied through the MCU platform. I would like to integrate a power management module in between the device and the components in order to independently switch on/off components using a software defined trigger (e.g. digital input). Please consider looking over the diagram to get a better understanding of what I'm trying to do.
Could such system be implemented? If so, what would be the required parts that I need to get for:
- Integrated PWR Switch
- Li-Ion Solar Charging Circuit
However, if my design is incorrect, could someone please suggest an alternative? Thank you so much for helping out.
Kind regards,